This is an analyzer sequence parameter which sets up the test set's analyzer to match the frequency of the signal it will be receiving. If the radio standard is other than NONE, this parameter specifies a channel number appropriate to the Standard, Band, and Device specified for the acquisition. If the radio standard is NONE, this parameter specifies a frequency in MHz.
There is no dropdown list for this field; it is necessary to enter a suitable value.